AXIS#.WS.TIRAMP
Description
In Wake & Shake mode 1, a maximum current of AXIS#.WS.IMAX is applied to the AXIS#.MOTOR. AXIS#.WS.TIRAMP defines a time to reach this maximum current. Longer times are useful for big inertia motors or heavy loads.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
ms |
Range |
512 to 10,000 |
Default Value |
512 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.WS.TIRAMP | 0x5013 | 0x11 | UINT | - | - | RW | False |
AXIS2.WS.TIRAMP | 0x5113 | 0x11 | UINT | - | - | RW | False |